The G3 MAC Wrapper module is located below the G3 Adaptation layer and on top of both PLC and RF MAC layers.
Its mission is to provide abstraction to upper layer (being G3 Adaptation layer or an application running on top of G3 MAC), to the fact that we are working on a PLC node, an RF node, or a Hybrid (PLC & RF) node.
Figure . MAC Wrapper Unified Access
Example application to send data from a G3 node at MAC level, and wait for a response
#defineSRC_PANID0X1234#defineSRC_ADDRESS0x0001#defineDEST_PANID0X1234#defineDEST_ADDRESS0x0002
SYS_MODULE_OBJ sysObjMacWrp;
MAC_WRP_HANDLE g3handle;
APP_G3_MAC_DATA appG3Mac;
bool txConfirmed;
bool frameReceived;
uint8_t txHandle;
uint8_t txBuffer[MAC_MAX_PAYLOAD_SIZE];
uint16_t txLength;
staticvoidAPP_SendData(uint8_t* pData, uint16_t length)
{
MAC_WRP_DATA_REQUEST_PARAMS drParams;
if (length > MAC_MAX_PAYLOAD_SIZE) {
return;
}
/* Prepare Data Request parameters */
drParams.srcAddressMode = MAC_WRP_ADDRESS_MODE_SHORT;
drParams.destPanId = DEST_PANID;
drParams.destAddress = DEST_ADDRESS;
drParams.msduLength = length;
drParams.msdu = pData;
drParams.msduHandle = txHandle++;
drParams.txOptions = 1;
drParams.securityLevel = MAC_WRP_SECURITY_LEVEL_ENC_MIC_32;
drParams.keyIndex = 0;
drParams.qualityOfService = MAC_WRP_QUALITY_OF_SERVICE_NORMAL_PRIORITY;
drParams.mediaType = MAC_WRP_MEDIA_TYPE_REQ_PLC_BACKUP_RF;
/* Send MAC Frame */
txConfirmed = false;
MAC_WRP_DataRequest(g3handle, &drParams);
}
staticvoidAPP_G3_MAC_DATACfmCb(MAC_WRP_DATA_CONFIRM_PARAMS *cfmObj)
{
/* Update flag */
txConfirmed = true;
}
staticvoidAPP_G3_MAC_DATAIndCb(MAC_WRP_DATA_INDICATION_PARAMS *indObj)
{
/* Do whatever with received frame */
frameReceived = true;
}
voidAPP_G3_MAC_Initialize(void)
{
/* Call system-like Initialize function */
sysObjMacWrp = MAC_WRP_Initialize(MAC_WRP_INDEX_0);
/* Set App state */
appG3Mac.state = APP_G3_MAC_STATE_IDLE;
}
voidAPP_G3_MAC_OpenAndInit(void)
{
/* Configure callbacks */
MAC_WRP_HANDLERS macWrpHandlers = {
.dataConfirmCallback = APP_G3_MAC_DATACfmCb,
.dataIndicationCallback = APP_G3_MAC_DATAIndCb,
.resetConfirmCallback = NULL, // Reset primitive not used
.beaconNotifyIndicationCallback = NULL, // BCN notify primitive not used
.scanConfirmCallback = NULL, // Scan primitive not used
.startConfirmCallback = NULL, // Start primitive not used
.commStatusIndicationCallback = NULL, // CommStatus primitive not used
.snifferIndicationCallback = NULL, // MAC Sniffer not used
};
/* Open an instance of module */
g3handle = MAC_WRP_Open(MAC_WRP_INDEX_0, MAC_WRP_BAND_CENELEC_A);
/* Set callbacks */
MAC_WRP_SetCallbacks(g3handle, &macWrpHandlers);
}
voidAPP_G3_MAC_Tasks(void)
{
/* Check the application's current state. */switch (appG3Mac.state)
{
case APP_STATE_IDLE:
{
/* Go to next state */
appG3Mac.state = APP_G3_MAC_STATE_OPEN_AND_INIT;
}
break;
case APP_G3_MAC_STATE_OPEN_AND_INIT:
{
/* Open and Init a MAC Wrapper instance */
APP_G3_MAC_OpenAndInit();
appG3Mac.state = APP_G3_MAC_STATE_SET_PARAMS;
}
break;
case APP_G3_MAC_STATE_SET_PARAMS:
{
/* Set own Address and PAN_ID */
MAC_WRP_STATUS status;
MAC_WRP_PIB_VALUE pibVal;
uint16_t panId = SRC_PANID;
uint16_t address = SRC_ADDRESS;
pibVal.length = 2;
memcpy(pibVal.value, &panId, sizeof(panId));
status = MAC_WRP_SetRequestSync(g3handle, MAC_WRP_PIB_PAN_ID, 0, &pibVal);
if (status == MAC_WRP_STATUS_SUCCESS)
{
memcpy(pibVal.value, &address, sizeof(address));
status = MAC_WRP_SetRequestSync(g3handle, MAC_WRP_PIB_SHORT_ADDRESS, 0, &pibVal);
if (status == MAC_WRP_STATUS_SUCCESS)
{
/* Go to next state */
appG3Mac.state = APP_G3_MAC_STATE_TX_REQUEST;
}
}
break;
}
case APP_G3_MAC_STATE_TX_REQUEST:
{
/* Build a frame in buffer and set length before calling SendData */
APP_SendData(txBuffer, txLength);
appG3Mac.state = APP_G3_MAC_STATE_WAITING_TX_CFM;
break;
}
case APP_G3_MAC_STATE_WAITING_TX_CFM:
{
if (txConfirmed)
{
frameReceived = false;
appG3Mac.state = APP_G3_MAC_STATE_WAITING;
}
break;
}
case APP_G3_MAC_STATE_WAITING:
{
if (frameReceived)
{
frameReceived = false;
/* Send another frame */
appG3Mac.state = APP_G3_MAC_STATE_TX_REQUEST;
}
break;
}
/* The default state should never be executed. */default:
{
/* Handle error in application's state machine. */break;
}
}
}