3.1.3 Building Linux System Image
Start the build operation using $ make command from the
buildroot-at91 directory.
Note: Ensure that the host PC is connected to the internet before
starting the build operation and do not use any build options.
Files get generated in the buildroot-at91/output/images directory when the build
operation is completed. The following figure shows the list of the generated files. The
sdcard.img is the whole image file which contains all necessary
modules to boot up the board.
The driver source files are located at
build/linux-custom/drivers/net/wireless/microchip/wilc1000.
Note: The driver directory name is WILC1000 for legacy reasons
only.