1.2.3 SCL and SDA Pins
Both TWI lines (SDA and SCL) are bi-directional, therefore outputs connected to the TWI bus must be of an open-drain or an open-collector type. Each line must be connected to the supply voltage via a pull-up resistor. A line is then logic high when none of the connected devices drives the line, and logic low if one or more drives the line low.
The output drivers contain a slew-rate limiter. The input stages contain a spike suppression unit removing spikes shorter than 50ns. Note that the internal pull-ups in the AVR pads can be enabled by setting the PORT bits corresponding to the SCL and SDA pins, as explained in the I/O Port section. In some systems, the internal pull-ups can eliminate the need for external resistors.
The following figure shows how to connect the TWI units to the TWI bus. The value of Rp depends on VCC and the bus capacitance, typically 4.7kΩ.