24.3.2.1.1 Normal Mode
In Normal mode, the system is single-buffered in the transmit direction and double-buffered
         in the receive direction. This influences the data handling in the following ways:
      - New bytes to be sent cannot be written to the DATA (SPIn.DATA) register before the entire transfer has been completed. A premature write will cause corruption of the transmitted data, and the Write Collision (WRCOL) flag in SPIn.INTFLAGS will be set.
 - Received bytes are written to the Receive Data Buffer register immediately after the transmission is completed.
 - The Receive Data Buffer register has to be read before the next transmission is completed, or the data will be lost. This register is read by reading SPIn.DATA.
 - The Transmit Data Buffer and Receive Data Buffer registers are not used in Normal mode.
 
After a transfer has been completed, the Interrupt Flag (IF) will be set in the Interrupt Flags (SPIn.INTFLAGS) register. This will cause the corresponding interrupt to be executed if this interrupt and the global interrupts are enabled. Setting the Interrupt Enable (IE) bit in the Interrupt Control (SPIn.INTCTRL) register will enable the interrupt.