3.2.2 Using the Library

Topics

Name Description
Abstraction Model Describes the abstraction model of the USB Host Layer.
Library Overview The USB Host layer API is grouped functionally, as shown in the following table.
How the Library Works Describes how the Library works and how it should be used.