2.6.3 Configuring the Library

The following configuration parameters must be defined while using the HID Function Driver. The configuration macros that implement these parameters must be located in the system_config.h file in the application project and a compiler include path (to point to the folder that contains this file) should be specified.

Macros

Name Description
USB_DEVICE_HID_INSTANCES_NUMBERSpecifies the number of HID instances
USB_DEVICE_HID_QUEUE_DEPTH_COMINEDDOM-IGONORE-BEGIN
Configuration on MCCThis section describes the symbols available in the MCC that can be configured