Name | Description |
Introduction
| Introduces the MPLAB Harmony USB Host Layer Library. |
Using the
Library | This topic describes the basic architecture of the USB Host Layer and
provides information and examples on its use. |
Configuring the Library
| Describes how to configure the USB Host Layer. |
Library
Interface
| This section describes the Application Programming Interface (API) functions
of the USB Host Layer Library.Refer to each section for a detailed description.
|
Files
| This section lists the source and header files used by the library. |