3.4 USB CDC Host Library

Topics

Name Description
IntroductionIntroduces the MPLAB Harmony USB CDC Host Library.
Using the LibraryThis topic describes the basic architecture of the USB CDC Host Client Driver Library and provides information and examples on its use.
Configuring the LibraryDescribes how to configure the USB CDC Host Library.
Library Interface This section describes the Application Programming Interface (API) functions of the USB CDC Client Driver Library. Refer to each section for a detailed description.
Files This section lists the source and header files used by the library.