1.3.5 SAMA7D65-Curiosity Board: Building and Running the OTA Bootloader With SD/eMMC Media Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file.

Path of the application within the repository is apps/ble/mpu/sama7d65_sd_emmc/.

To build the application, refer to the following table and open the project using its IDE.

OTA Bootloader

Project NameDescription
ota_bootloader/sam_a7d65_curiosity.XMPLABX Project for SAMA7D65-Curiosity Board

OTA Application

Project NameDescription
ota_app/sam_a7d65_curiosity.XMPLABX Project for SAMA7D65-Curiosity Board

Setting Up SAMA7D65-Curiosity Board

  • To run the demo, the following additional hardware are required:

  • Short J2-1 and J2-2 using jumper in the RNBD451 Add On Board

  • Insert RNBD451 Add On Board board into MIKROBUS 1 Connector

  • Connect the UART Debug port (J35) on the target curiosity board to the computer using a FTDI-USB cable

  • Connect the USBA port J3 on the target curiosity board to the computer using a Type-C USB cable (to power the board)

  • SD Card with FAT32 file system for curiosity board

Setting Up the Host Scripts

Running the Application

  1. Open the Terminal application (Ex.:Tera Term) on the computer.

  2. Configure the serial port settings as follows:

    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  3. Open the bootloader project ota_bootloader/sam_a7d65_curiosity.X in the IDE.

  4. Build the project to generate the harmony_bootloader.bin binary (Do not program the binary).

  5. Open the application project ota_app/sam_a7d65_curiosity.X in the IDE.

  6. Build the project to generate the harmony.bin binary (Do not program the binary).

  7. Copy the MPU bootstrap loader binary (boot.bin) from <harmony3_path>/bootloader_apps_ota/deps/at91bootstrap_binaries_sam_a7d65_curiosity/bootloader/sd_card/boot.bin onto the SD Card.

  8. Copy the harmony bootloader binary (harmony_bootloader.bin) from <harmony3_path>/bootloader_apps_ota/apps/ble/mpu/sama7d65_sd_emmc/ota_bootloader/sam_a7d65_curiosity.X/dist/default/production/harmony_bootloader.bin onto the SD Card.

  9. Copy the ota application binary (harmony.bin) from <harmony3_path>/bootloader_apps_ota/apps/ble/mpu/sama7d65_sd_emmc/ota_app/sam_a7d65_curiosity.X/dist/default/production/harmony.bin onto the SD Card.

  10. Insert the SD card into SD CARD connector on the curiosity board.

  11. Reset or Power cycle the device. Green LED will be blinking to indicate that the OTA application is running.

    • Observe the below message on console:
    console_output1
  12. Open the OTA application project ota_app/sam_a7d65_curiosity.X in the IDE.

  13. Update ota_app/src/app.c to update printf() message from ####### Application running ####### to ####### New Application running ####### as below:

    app_source
  14. Clean and Build the OTA application project to generate the binary (Do not program the binary).

  15. Go to the <harmony3_path>/bootloader_apps_ota/apps/ble/mpu/sama7d65_sd_emmc/ota_app/sam_a7d65_curiosity.X/dist/default/production/ directory and open the command prompt to run the below command:

    python <harmony3_path>/bootloader_apps_ota/tools/ota_host_mcu_header.py -p 0x0 -j 0x0 -l 0x0 -f harmony.bin
    • This command adds OTA Host MCU Header to the application binary. If command executed successful then "image.bin is generated successfully" message display on the command prompt.
    • Note: Memory addresses are configured from MCC harmony and it is not used from above command.
  16. Run the below command:

    python <harmony3_path>/bootloader_apps_ota/tools/ota_rnbd_header.py -f image.bin
    • This command adds OTA RNBD Header to the image.bin and generates RNBD_image.bin application binary. If command executed successful then "RNBD_image.bin is generated successfully" message display on the command prompt.
  17. Refer to the Send application binary using MBD App to program RNBD_image.bin application binary to the target.

  18. Once Firmware Update is successful:

    • Green LED still blinking indicating that the OTA application is running
    • Observe the below message on console:
    console_output2
  19. Repeat Step 13-18.

    • Observe Green LED still blinking
    • Observe message printed on console

Additional Steps (Optional)

  • If required, the following commands need to be executed to set up boot configuration on the SAMA7D65 Curiosity board:

    sam-ba -p usb -d sama7d65 -a bootconfig -c writecfg:bscr:EMULATION_ENABLED

    sam-ba -p usb -d sama7d65 -a bootconfig -c resetemul

    sam-ba -p usb -d sama7d65 -a reset

    sam-ba -p usb -d sama7d65 -a bootconfig -c writecfg:bcp-otp:FLEXCOM6_USART_IOSET4,QSPI0_IOSET1_AT25,NFC_IOSET1_PMECC0xc2605007,SDMMC1_IOSET1

  • To bootload any other application refer to the Configuring an application to be bootloaded for MPUs