1.2.3 PIC32MK MCM Curiosity Pro Development Board: Building and Running the UART Fail Safe Bootloader applications

Downloading and building the application

To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions

Path of the application within the repository is apps/uart_fail_safe_bootloader/

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader/firmware/pic32mk_mcm_curiosity_pro.XMPLABX Project for PIC32MK MCM Curiosity Pro Development Board

Test Application

Project NameDescription
test_app/firmware/pic32mk_mcm_curiosity_pro.XMPLABX Project for PIC32MK MCM Curiosity Pro Development Board

Setting up PIC32MK MCM Curiosity Pro Development Board

  • Connect a micro USB cable to the USB to UART port J400. This will enumerate as a COM port on the PC.
  • For programming, Connect a micro USB cable to the USB DEBUG port J500

Setting up the host script

Running the Application

  1. Open the test application project test_app/firmware/pic32mk_mcm_curiosity_pro.X in the IDE

  2. Build the project to generate the binary (Do not program the binary)

  3. Open the bootloader project bootloader/firmware/pic32mk_mcm_curiosity_pro.X in the IDE

  4. Build and program the application using the IDE

  5. Run the btl_host.py from command prompt to program the test application binary to opposite panel

     python <harmony3_path>/bootloader/tools/btl_host.py -v -s -i <COM PORT> -d pic32mk -a 0x9D080000 -f <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/test_app/firmware/pic32mk_mcm_curiosity_pro.X/dist/pic32mk_mcm_curiosity_pro/production/pic32mk_mcm_curiosity_pro.X.production.bin
  6. Following snapshot shows output of successfully programming the test application

    • Swapping Bank And Rebooting and Reboot Done messages in below output signifies that bootloading is successful
    output
  7. If above step is successful then the LED3 should start blinking

  8. Open the Terminal application (Ex.:Tera Term) on the computer

  9. Configure the serial port settings as follows:

    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  10. Reset or Power cycle the device

  11. LED3 should start blinking and you should see below output on the console

    • The Program Flash Bank Can be BANK 1 or BANK 2 based on from where the program is running
    output
    output
  12. Press and hold the Switch SW1 to trigger Bootloader from test application to program firmware in other bank and you should see below output

    output
  13. Repeat Steps 5-11 once

    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 12
    • Also to program the new firmware in opposite bank
    • You should see other Bank in console displayed compared to first run

Additional Steps (Optional)