1.2.6 SAM E54 Xplained Pro Evaluation Kit: Building and Running the UART Fail Safe Bootloader applications

Downloading and building the application

To clone or download this application from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions

Path of the application within the repository is apps/uart_fail_safe_bootloader/

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader/firmware/sam_e54_xpro.XMPLABX Project for SAM E54 Xplained Pro Evaluation Kit

Test Application

Project NameDescription
test_app/firmware/sam_e54_xpro.XMPLABX Project for SAM E54 Xplained Pro Evaluation Kit

Setting up SAM E54 Xplained Pro Evaluation Kit

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Setting up the host script

Running the Application

  1. Open the test application project test_app/firmware/sam_e54_xpro.X in the IDE

  2. Build the project to generate the binary (Do not program the binary)

  3. Open the bootloader project bootloader/firmware/sam_e54_xpro.X in the IDE

  4. Build and program the application using the IDE

  5. Launch MCC for the bootloader/firmware/sam_e54_xpro.X project

    • Disable Fuse Settings

      mhcSetting
    • Regenerate the project

    • Enable Execute this line After Build option in MPLAB X Project properties->Building option

      buildOption
  6. Build the project to generate the bootloader binary (Do not program the binary)

  7. Run the btl_app_merge_bin.py from command prompt to merge the generated Bootloader binary and test application binary. Below output should be displayed on command prompt

     python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o 0x2000 -b <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/bootloader/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin -a <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/test_app/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin
    output
  8. Run the btl_host.py from command prompt to program the merged binary to opposite panel. btl_app_merged.bin will be created in the current directory from where the btl_app_merge_bin.py was called

     python <harmony3_path>/bootloader/tools/btl_host.py -v -s -i <COM PORT> -d same5x -a 0x80000 -f <Path_To_Merged_Binary>/btl_app_merged.bin
  9. Following snapshot shows example output of successfully programming the merged binary

    • Swapping Bank And Rebooting and Reboot Done messages in below output signifies that bootloading is successful
    output
  10. If above step is successful then the LED0 should start blinking

  11. Open the Terminal application (Ex.:Tera Term) on the computer

  12. Configure the serial port settings as follows:

    • Baud : 115200
    • Data : 8 Bits
    • Parity : None
    • Stop : 1 Bit
    • Flow Control : None
  13. Reset or Power cycle the device

  14. LED0 should start blinking and you should see below output on the console

    • The NVM Flash Bank Can be BANK A or BANK B based on from where the test application is running
    output
    output
  15. Press and hold the Switch SW0 to trigger Bootloader from test application to program firmware in other bank and you should see below output

    output
  16. Disconnect UART console

  17. Run the btl_host.py from command prompt to program only the test application binary to opposite panel

    python <harmony3_path>/bootloader/tools/btl_host.py -v -s -i <COM PORT> -d same5x -a 0x82000 -f <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/test_app/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin
  18. Repeat Steps 9-14 once

    • This step is to verify that bootloader is running after triggering bootloader from test application in Step 15
    • Also to program the new firmware in opposite bank
    • You should see other Bank in console displayed compared to first run

Note:

If demo needs to be restarted from beginning

  • Revert the changes done in Step 5
  • Regenerate the project
  • Start from Step 4

Additional Steps (Optional)