1.3.2 SAM9X75 Curiosity Board: Building and Running the UART Bootloader With SD/eMMC Media Applications

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using content manager by following these instructions.

Path of the application within the repository is apps/mpu_uart_bootloader/.

To build the application, refer to the following table and open the project using its IDE.

Bootloader Application

Project NameDescription
bootloader_sd_emmc/firmware/sam_9x75_curiosity.XMPLAB X Project for SAM9X75 Curiosity Board

Test Application

Project NameDescription
test_app/firmware/sam_9x75_curiosity.XMPLAB X Project for SAM9X75 Curiosity Board

Setting Up SAM9X75 Curiosity Board

  • Connect the DBGU0 J35 on board to the computer using a UART-FTDI cable (to enable debug com port)
  • Connect the USB port J2 on board to the computer using a micro USB cable (to power the board)
  • SD card with FAT32 file system

Setting Up the Host Script

Running the Application

  1. Open the test application project test_app/firmware/sam_9x75_curiosity.X in the IDE.

  2. Build the project to generate the harmony.bin binary (Do not program the binary).

  3. Open the bootloader project bootloader_sd_emmc/firmware/sam_9x75_curiosity.X in the IDE.

  4. Build the project to generate the harmony_bootloader.bin binary (Do not program the binary).

  5. Copy the MPU bootstrap loader binary (boot.bin) from <harmony3_path>/bootloader_apps_uart/deps/at91bootstrap_binaries_sam_9x75_curiosity/sd_card/boot.bin onto the SD card.

  6. Copy the harmony bootloader binary (harmony_bootloader.bin) from <harmony3_path>/bootloader_apps_uart/apps/mpu_uart_bootloader/bootloader_sd_emmc/firmware/sam_9x75_curiosity.X/dist/sam_9x75_curiosity/production/harmony_bootloader.bin onto the SD card.

  7. Insert the SD card into SD BOOT connector J14 on the board.

  8. Reset or Power cycle the device. Green LED will be turned-on to indicate that harmony bootloader code is running on the target.

  9. Run the btl_host.py from command prompt to program the application binary.

     python <harmony3_path>/bootloader/tools/btl_host.py -v -i <COM PORT> -d sam9x7 -f <harmony3_path>/bootloader_apps_uart/apps/mpu_uart_bootloader/test_app/firmware/sam_9x75_curiosity.X/dist/sam_9x75_curiosity/production/harmony.bin
    
  10. Following figure shows output of successfully programming the test application.

    • Rebooting and Reboot Done messages in below output signifies that bootloading is successful
  11. If above step is successful then the Green LED should start blinking.

  12. Open the Terminal application (e.g., Tera Term) on the computer.

  13. Configure the serial port settings as follows:

    • Baud: 115200
    • Data: 8 Bits
    • Parity: None
    • Stop: 1 Bit
    • Flow Control: None
  14. Reset or Power cycle the device.

  15. Green LED should start blinking and the user should see below output on the console.

  16. Press and hold the Switch USER and then press Reset button or Power cycle the device to force trigger bootloader at startup.

  17. Repeat Steps 9-15 once.

    • This step is to verify whether bootloader is triggered by switch press at reset