1.4.1 Bootloader and Application Binary Merge Script Help

This document describes the usage of btl_app_merge_bin.py host script.

Path of the tool in bootloader repository is tools/btl_app_merge_bin.py.

Setting Up the Host PC

The Script is compatible with Python 3.x and higher.

Description

  • This script should be used to merge the bootloader binary and application binary

  • It creates a merged binary output where bootloader is placed from start and the application will be placed at the offset passed as parameter

  • If the application offset is not equal to end of bootloader offset it fills the gap with 0xFF until the application offset

  • The merged binary can be used by btl_host.py as input for Updating bootloader and application together

  • The merged binary will be created in the directory from where the script was called

Usage Examples

Below is the syntax to show help menu for the script:

python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py --help

Below is the syntax and an example on how to merge a bootloader binary and application binary:

python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o <Offset> -b <Bootloader_binary_path> -a <Application_binary_path>
python <harmony3_path>/bootloader/tools/btl_app_merge_bin.py -o 0x2000 -b <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/bootloader/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin -a <harmony3_path>/bootloader_apps_uart/apps/uart_fail_safe_bootloader/test_app/firmware/sam_e54_xpro.X/dist/sam_e54_xpro/production/sam_e54_xpro.X.production.bin
python <harmony3_path>/bootloader/tools/btl_host.py -v -s -i COM18 -d same5x -a 0x80000 -f <Path_to_merged_binary>/btl_app_merged.bin