3.4 Build the Linux Image
After all the required changes are made, the building can be performed.
- Navigate to the buildroot-at91
directory:
$ cd buildroot-at91 - Build the Linux image with the
following command:Note: Before building the buildroot-at91, setup the cross-compile toolchain. Refer to the cross compiler section for additional instructions.
$ makeThe building process will take a few hours to complete.
- Once the build is complete, navigate to buildroot-at91/output/Images.
- Verify that the sdcard.img file is generated.