5.3.1 Word Address Values

During an I/O write packet, the TA010-TFLXWPC interprets the second byte sent as the word address, which indicates the packet function as it is described in the table below:

Table 5-2. Word Address Values
NameValueDescription
Reset0x00Resets the address counter. The next I/O read or write transaction will start with the beginning of the I/O buffer.
Sleep 
(low-power)0x01 or 0x02The TA010-TFLXWPC goes into the low-power Sleep mode and ignores all subsequent I/O transitions until the next Wake flag. The entire volatile state of the device is reset.
Command0x03Writes subsequent bytes to sequential addresses in the input command buffer that follow previous writes. This is the normal operation.
Note: Only the lower two bits of the Word Address byte are decoded by the TA010-TFLXWPC.