1.6.2 SAMD11 Xplained Mini Onboard Sensor Example
Path of the application within the repository is apps/onboard_sensor/firmware/sam_d11_xmini/
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
|
firmware\sam_d11_xmini.X | MPLABX Project for SAM D11 Xplained Pro Evaluation Kit |
Hardware Setup
- Project uses SAM D11 Xplained Pro Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
- This project supports two on-board touch buttons available in the evaluation kit
Running The Application
- Open the application project sam_d11_xmini.X in the IDE
- Build the project and program the target board
Monitoring Touch Data in MPLAB DV Touch Plugin
Prerequisite: MPLAB Data Visualizer and Touch Plugin. Procedure for Installation is available in Touch Plugin Installation.
- Configure COM Port
- Select the correct COM port in Connection tab
- Update the Baud Rate to 115200 in COM Settings
- Start Streaming for COM data
- COM Port on Touch
- Select Touch in Connection tab
- For data source, from drop-down menu, select configured COM port as source
- Start Streaming on Touch
Detailed procedure can be found in Guide to view Touch Tune Data using MPLAB® Data Visualizer page.