The DALI Bus connector is dedicated for the DALI bus.
The DALI bus is a pair of cables, which can connect the DALI Master and all DALI Slaves. Since the DALI bus carries the differential signal, the users need not to take care of the polarity of the connection.
Strip the DALI bus cable in both ends first. Push the socket header on the top, then insert the cable to the hole, and release the header. The cable will be locked in the socket.
The accomplished figure should look like the figure below.