The Graph module is a versatile graph plotting tool. The large plot area has one time axis, and one or more value axes (Y axes). The value axes are stacked on top of each other. For an example on how to configure a graph, see Graph Configuration Example.
There are four types of elements that can be added to an Y axis:
Plot
Band
String marker
Horizontal cursor
Each of these elements are described in the following sections.