8.6 SIGROW - Signature Row

The content of the Signature Row (SIGROW) fuses is preprogrammed and read-only. SIGROW contains information such as device ID, serial number, and calibration values.

All the AVR32/16DD14/20 devices have a three-byte device ID that identifies the device. The device ID can be read using the Unified Program and Debug Interface (UPDI), also when a device is locked. The device ID for the AVR32/16DD14/20 devices consists of three signature bytes, as shown in the following table.

Table 8-4. Device ID
Device Name Signature Byte Address and Value
0x00 0x01 0x02
AVR32DD32 0x1E 0x95 0x38
AVR32DD28 0x1E 0x95 0x39
AVR16DD32 0x1E 0x94 0x31
AVR16DD28 0x1E 0x94 0x32