45.4 Signal Description

Pin NameTypeDescription
TCC/WO[0]Digital outputCompare channel 0 waveform output
TCC/WO[1]Digital outputCompare channel 1 waveform output
…......
TCC/WO[7]Digital outputCompare channel 7 waveform output
CAUTION: I/Os for TCC peripheral are grouped into I/O sets, listed in their `IOSET' column in the pinout tables.

For these peripherals, it is mandatory to use I/Os that belong to the same I/O set. The timings are not guaranteed when I/Os from different I/O sets are mixed. Refer to the Pinout and Packaging chapter to get IOSET definitions.