4.1.2 bmm_buffer_alloc Function
C
buffer_t* bmm_buffer_alloc(uint16_t size)
Summary
Allocates a buffer
Description
This function allocates a buffer and returns a pointer to the buffer. The same pointer should be used while freeing the buffer.User should call BMM_BUFFER_POINTER(buf) to get the pointer to buffer user area
Precondition
bmm_buffer_init should have been called before using this function
Parameters
| Param | Description |
|---|---|
| size | size of buffer to be allocated |
Returns
return- pointer to the buffer allocated, NULL if buffer not available
Example
buffer_t *buffer;
buffer = bmm_buffer_alloc(LARGE_BUFFER_SIZE);
if (buffer == NULL)
{
//Buffer is unavailable
}
Remarks
This routine is used by the PHY Layer for allocating the buffer for reception. Number of Buffers should be defined as per application needs before the buffer allocation function. If application allocates the buffer and not freeing them, Trx may not able to continuously receive the packet. So care should be taken when defining the Number of Buffers.