6.10.4 localeconv Function
Sets the components of an structure with locale-specific values appropriate for the formatting of numeric quantities.
"C" locale is
supported.Include
<locale.h>
Prototype
struct lconv * localeconv(void);
Return Value
The function returns a pointer to the completed object, which shall not be modified by
the program, but may be overwritten by a subsequent call to this function. In addition,
calls to the setlocale() function with categories
LC_ALL, LC_MONETARY, or
LC_NUMERIC may overwrite the contents of the structure.
Remarks
The function sets the components of a structure with locale-specific values appropriate
for the formatting of numeric quantities. Structure members of type char
* (with the exception of decimal_point) can point to
"", to indicate that the value is not available in the current
locale or is of zero length. Apart from grouping and
mon_grouping, the strings shall start and end in the initial shift
state. The members with type char are non-negative numbers, any of
which can be CHAR_MAX to indicate that the value is not available in
the current locale.
Those MPLAB XC compilers that implement setlocale() only support the
"C", which specifies the minimal environment for C translation.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <locale.h>
struct lconv * ll;
int main(void) {
ll = localeconv();
setlocale(LC_ALL, "C");
}