6.13.10 signal Function
Controls interrupt signal handling.
Include
<signal.h>
Prototype
void (*signal(int sig, void(*func)(int)))(int);
Arguments
sig- signal name
func- function to be executed
Return Value
Returns the previous value of func.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
Note that the raise() function is only implemented as a stub when using
MPLAB XC32.
#include <signal.h>
#include <stdio.h>
/* Signal handler function */
void mysigint(int id)
{
printf("SIGINT received\n");
}
int main(void)
{
/* Override default with user defined function */
signal(SIGINT, mysigint);
raise(SIGINT);
/* Ignore signal handler */
signal(SIGILL, SIG_IGN);
raise(SIGILL);
printf("SIGILL was ignored\n");
/* Use default signal handler */
raise(SIGFPE);
printf("Program never reaches here.");
}
Example Output
SIGINT received
SIGILL was ignored
FPE
Example Explanation
The function mysigint is the user-defined signal handler for
SIGINT. Inside the main program, the function signal is called to
set up the signal handler (mysigint) for the signal
SIGINT that will override the default actions. The function raise
is called to report the signal SIGINT. This causes the signal handler
for SIGINT to use the user-defined function (mysigint)
as the signal handler so it prints the “SIGINT received” message.
Next, the function signal is called to set up the signal handler SIG_IGN
for the signal SIGILL. The constant SIG_IGN is used to
indicate the signal should be ignored. The function raise is called to report the signal
SIGILL that is ignored.
The function raise is called again to report the signal SIGFPE. Since
there is no user-defined function for SIGFPE, the default signal
handler is used so the message “FPE” is printed (which stands for “arithmetic error -
terminating”). Then, the calling program is terminated. The printf
statement is never reached.