4 Running the Demo
The PolarFire Evaluation Board comes with a preprogrammed JESD204B standalone demo design. The demo operates in loopback mode to establish a standalone JESD interface demo that does not require analog-to-digital (ADC) or digital-to-analog converters (DAC) by looping data between the TX and RX IP cores for JESD204B.
In order to run the demo, install the JESD204B_GUI application and set up the board as
outlined in the following steps. For detailed instructions, see DG0755 (PolarFire FPGA JESD204B Standalone
Interface Demo Guide).
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the host PC to the J5 connector (FTDI port) on the board.
- Power on the board using the SW3 slide switch.