25.8.4 CLB Configuration Steps
Configuration of the CLB consists of the following steps:
- Determine which of the CLB
configuration modes will be used:
- CPU executes code to configure the CLB
- Automatic Configuration on Start-up mode with CPU execution
- Automatic Configuration on Start-up mode with CPU halt
- Create the CLB bitstream using
the Microchip CLB Synthesizer:
- Select the inputs into the CLB using the CLB Input Selection latches
- Configure input edge detection and synchronization using the CLB Input Synchronizer latches
- Select the inputs into the BLEs using the BLE Input Selection latches
- Configure the BLE LUTs with entries corresponding to each expected input combination using the CLB LUT latches
- Configure output edge detection and synchronization using the CLB Output Synchronizer latches
- Configure the BLE output flops using the BLE Flop Select latches
- Configure the CLB interrupts using the CLB Interrupt Selection latches
- Determine which BLE output is routed to the sixteen PPS outputs using the CLB Output Selection latches
- Determine which BLE output is routed to the CLB Software Output Registers by configuring CLBSWOUTH and CLBSWOUTL.
- Configure the CLB inputs to any peripherals used by the application.
- Configure CLB outputs using the CLBPPSOUT registers (see the "Peripheral Pin Select (PPS)" chapter).
- Select the CLB clock source and clock prescaler using the CLBCLK register.
-
- If the “CPU executes code
to configure the CLB” mode is used:
- Transfer the CLB bitstream to program memory using the Microchip CLB Synthesizer
- Configure the NVM Scanner to interact with the CLB module (refer to the “CRC” chapter for more details)
- Enable the scanner to load the CLB netlist values into the CLB latches
- Once the scanner has loaded the CLB configuration into NVM, enable the CLB module by setting the EN bit.
- If either of the
Automatic Configuration on Start-up modes are used:
- Configure any other peripherals that are used by the application(1)
- Ensure that the high address byte of the location in program memory of the CLB bitstream is loaded into the CLBSA bits of the Configuration Words
- Transfer the CLB bitstream to program memory using the Microchip CLB Synthesizer
- Enable the CLB module by setting the EN bit
- If the “CPU executes code
to configure the CLB” mode is used:
Note:
- When
CPUHALT =
1, the CLB module SFRs should also be configured in the same start-up routine as the other peripherals used in the application. Peripherals that are enabled during 'Automatic Configuration on Start-up with CPU execution' mode will begin to operate immediately. If application code reconfigures a peripheral while it is enabled, unpredictable operation may occur.
The outputs of the CLB can be viewed through external pins via PPS, or by reading the CLBSWOUTH, CLBSWOUTL, CLBOUTH, and/or CLBOUTL registers. The CLB outputs are also internally connected to other peripherals.