5.1.3.1 SlotLock

The Slot Lock mode of the Lock command is used to individually lock slots. Any slot that has the Lockable bit set and has not previously been slot-locked can be locked to prevent any further updates. This process is not reversible. Once a slot has been locked, it is permanently locked. In this mode of operation, the Summary CRC and Data fields are ignored.

For the ATECC608B-TNGLoRaWAN, the following individual slots may be locked: Slots 8, 10 and 14.

Table 5-10. SlotLock Input Parameters

Opcode
(1 Byte)

Mode

(1 Byte)

Summary CRC
(2 Bytes)

Data
(0 Bytes)

Description
0x178’b00[bb_bb]10(1)0x00 00—Individual Slot Lock
Note: 1 - [bb_bb] Indicates the 4-bit value that represents the slot being locked.
Table 5-11. Slot Lock Output
NameSizeDescription
Response1 byte0x00 if the command successfully locks the slot. An error code will output if the command fails.