5.2 Running Pose Estimation on GPU
To run this example, perform the following steps:
- Open a new terminal and navigate to
the
holoscan-sensor-bridgefolder by using the following command.cd <PATH/TO/holoscan-sensor-bridge> - The next step involves downloading
ffmpeg and ultralytics packages to run
the pose estimation demo from Running Holoscan Sensor Bridge examples - NVIDIA
Docs. Rather than going to the link above, type the following in the console
apt-get update && apt-get install -y ffmpeg pip3 install ultralytics onnx cd examples yolo export model=yolov8n-pose.pt format=onnx cd -Note:This conversion step only needs to be executed once; the yolov8n-pose.onnx file contains the converted model and is all that’s needed for the demo to run. The installed components will be forgotten when the container is exited; those do not need to be present in future runs of the demo.
- To run the sensor bridge
demonstration container, from a terminal in the GUI, Note: Ignore the step if the docker is running already
xhost + sh docker/demo.sh - To run the pose estimation
demo,
python examples/linux_imx477_pose_estimation.py - Close the Holoviz application and exit the docker to terminate the application