4.2 Programming using FlashPro Express
This is a faster method to program the board. This section describes how to program the
PolarFire® device using a .job file included in the design files by utilizing the
FlashPro Express software. The mpf_an5522_v2024p2_jb file is available
at the following location: <download_folder>\
mpf_an5522_v2024p2_jb.zip.
To program the PolarFire device with the .job file, perform the
following steps:
- Connect the USB Type-C cable from Host PC to J8 of MPF200-ETH-SENSOR-BRIDGE.
- On the Host PC, start the FlashPro Express software from its installation directory.
- To create a new job project on the Project menu, click New or New Job Project from FlashPro Express Job.
- In the New Job Project
from FlashPro Express Job dialog box, perform the following steps:
- Programming job file:
Click Browse, navigate to the location where
the
mpf_an5522_v2024p2_jbfile is located, and select the file. -
FlashPro Express job project location: Click Browse and navigate to the location where you want to save the project.
Figure 4-1. New Job Project from FlashPro Express Job
- Programming job file:
Click Browse, navigate to the location where
the
- Click OK. The required programming file is selected and ready to be programmed in the device. The FlashPro Express window appears.
- Verify that a programmer number appears in the Programmer box. If it does not, verify the board connections and click Refresh/Rescan Programmers.
- To program the device, click
Run. When the device is programmed successfully, a "Run"
status is displayed, as shown in the following figure.
Figure 4-2. FlashPro Express—RUN PASSED - To Close FlashPro Express, click Project > Exit. The PolarFire device is programmed.