6.4 Adding Custom Linker Script to MPLAB Harmony v3 Project
The MPLAB Harmony v3 project uses a default linker script that comes with MPLAB X IDE installation. A few projects might need custom linker scripts. The MPLAB Harmony v3 supports adding custom linker scripts to a project. Use the following steps to include the correct linker script in the project:
- Right-click on the Linker Files folder in project > Add Existing item > select specific linker script which needs to be linked.
- Project Properties > XC32
global options > xc32-ld > Additional options > add linker switch
to use the following linker file for linking,
[-T ..\..\..\yy\xxxx.ld].