6.3 Import Atmel START Project into MPLAB X IDE
Follow these steps to import the Atmel START project into the MPLAB X IDE:
- Open MPLAB X IDE.
- Select file > Import > START MPLAB Project.
- Upload the
.atzipfile using the Browse option. - Ensure that the correct device has been selected, choose the programming tool.
- Select the compiler toolchain as Arm.
- Specify the location of the project and verify all the information is accurate.