5.4 Downloading and Executing the Application
The firmware corresponding to this application note is available at www.atmel.com. The
following steps will explain how to program and execute this application.
- Open the project in Atmel Studio and compile it. Refer section Demo Project for more information on how to open the solution in Atmel Studio.
- To program the target device, go
to Project > Project
Properties>Tools tab. Select the tool
as mEDBG and interface as
debugWire as shown in the following image.
Figure 5-4. Tool and Interface Configuration for Programming
- To begin programming, click
Start Without Debugging in the toolbar as shown in
the following image.
Figure 5-5. Programming the Device
- To debug the code, go to
Tools tab. Select mEDBG as
Debugger/Programmer with debugWire Interface as in shown
in the following image.
Figure 5-6. Tool and Interface Configuration for Debugging
- To start debugging, click
Start Debugging in the toolbar as shown in the
following image.
Figure 5-7. Debugging the Device