5 Demo Project
The demo code associated with this application note is available as compressed zip file in Atmel Website.
To load the code in the Atmel Studio,
- Extract the zip file to get the project and associated source code.
- Start Atmel Studio, go to
File > Open and click on
Project/Solution. The shortcut key is (CTRL + Shift +
O).
Figure 5-1. Opening Example Project in Atmel Studio
- Open Project Dialog box will appear.
- Select the Example project solution file (.atsln) and click Open.
- Alternate method is to double click the (.atsln) file from the extracted folder, this action will start Atmel Studio and then load the project.