6 Transform Functions
| Function | Description |
|---|---|
| BitReverseComplex |
Reorganizes, in place, the elements of a complex vector in bit-reverse order. |
| CosFactorInit |
Generates the first half of the set of cosine factors required by a Type II Discrete Cosine Transform and places the result in the complex destination vector. |
| DCT |
Computes the Discrete Cosine Transform of a source vector and stores the results in the destination vector. |
| DCTIP |
Computes the Discrete Cosine Transform of a source vector in place. |
| FFTComplex |
Computes the Fast Fourier Transform of a source complex vector and stores the results in the destination complex vector. |
| FFTComplexIP |
Computes the Fast Fourier Transform of a source complex vector in place. |
| IFFTComplex |
Computes the Inverse Fast Fourier Transform of a source complex vector and stores the results in the destination complex vector. |
| IFFTComplexIP |
Computes the Inverse Fast Fourier Transform of a source complex vector in place. |
| FFTRealIP |
Performs an in-place Fast Fourier Transform (FFT) on a real-valued source vector. It utilizes an efficient algorithm that computes the FFT of a 2N-point real vector by leveraging an N-point complex FFT, supplemented with additional operations known as split functions. |
| FFTReal |
Performs Fast Fourier Transform (FFT) on a real-valued source vector and stores the result in a complex destination vector. It utilizes an efficient algorithm that computes the FFT of a 2N-point real vector by leveraging an N-point complex FFT, supplemented with additional operations known as split functions. |
| IFFTRealIP |
Computes, in place, the inverse Fast Fourier Transform of a source complex vector, which was derived out a real-vector using the FFTReal function. The algorithm to compute IFFT is based on the efficient computation of IFFT of a 2N point complex vector using the N point complex FFT with additional computations called split functions. |
| IFFTReal |
Computes the inverse Fast Fourier Transform of a source complex vector, which was derived out of a real-vector using the FFTReal function. The algorithm to compute IFFT is based on the efficient computation of IFFT of a 2N point complex vector using the N point complex FFT with additional computations called split functions. |
| SquareMagnitudeComplex |
Computes the squared magnitude of each element in a complex source vector. |
| TwidFactorInit |
Generates the first half of the set of twiddle factors required by a Discrete Fourier Transform or Discrete Cosine Transform, and places the result in the complex destination vector. |