2 Vector Functions
|
Function |
Description |
|---|---|
| VectorAdd | Adds the value of each element in the source one vector with its counterpart in the source two vector and places the result in the destination vector. |
| VectorConvolve | Computes the convolution between two source vectors and stores the result in a destination vector. |
| VectorCopy | Copies the elements of the source vector into the beginning of an (already existing) destination vector. |
| VectorCorrelate | Computes the correlation between two source vectors and stores the result in a destination vector. |
| VectorDotProduct | Computes the sum of the products between corresponding elements of the source one and source two vectors. |
| VectorMax | Returns the value and index of the last element in the source vector whose value is greater than or equal to any previous vector element. |
| VectorMin | Returns the value and index of the last element in the source vector whose value is lesser than or equal to any previous vector element. |
| VectorMultiply | Multiplies the value of each element in the source one vector with its counterpart in the source two vector and places the result in the corresponding element of destination vector. |
| VectorNegate | Negates (changes the sign of) the values of the elements in the source vector and places them in the destination vector. |
| VectorPower | Computes the power of a source vector as the sum of the squares of its elements. |
| VectorScale | Scales (multiplies) the values of all the elements in the source vector by a scale value and places the result in the destination vector. |
| VectorSubtract | Subtracts the value of each element in the source one vector with its counterpart in the source two vector and places the result in the destination vector. |
| VectorZeroPad | Copies the contents of the source vector into the beginning of the destination vector, and then fills the remaining positions—specified by numZeros — with zeros to complete the destination vector. |