1.2.2.1 Introduction
Simulator stimuli is a way to write simple script files that can read or write any register or memory location at a given time during the simulation. The stimuli file can be started at any time during the simulation and will continue until the end of the file or when the simulator session ends.
Starting with Atmel Studio 6.1, the File Stimulator found in AVR® Studio 4 has been reintroduced. There were two stimuli variants in AVR Studio 4. This is the most recent one used in Simulator 2. The older one is not supported.
Features of the File Stimulator:
-
Timing is expressed in terms of delay instead of absolute cycle counter values
-
Any I/O register can be assigned to (stimulated), not only port registers
-
Individual bits in I/O registers can be stimulated using bitwise assignments
-
Directives increase flexibility
One stimuli file can open and execute another stimuli file