5 Conclusion
This technical brief provides an overview of using the UART with the protocol support module in the DMX mode. It explains how the new module is beneficial in handling the timing requirements for the DMX protocol. The sample code snippets serve as a walk-through on how to get started in building an application that uses the DMX module. This technical brief also shows how the DMA module can be setup to transmit and receive data without the involvement of the CPU. For more information about this module, refer to the device data sheet.