9.8.1 Const Type Qualifier
The compiler supports the use of the ANSI type qualifiers
const and volatile.
The const type qualifier is used to tell the compiler
that an object is read only and will not be modified. If any attempt is made to modify an
object declared const, the compiler will issue a warning or error.
User-defined objects declared const are placed, by
default, in the program space. Usually a const object must be initialized
when it is declared, as it cannot be assigned a value at any point at runtime. For
example:
const int version = 3;
will define version as being an int
variable that will be placed in the program memory, will always contain the value 3, and
which can never be modified by the program.
The memory model -mconst-in-data will allocate
const-qualified objects in data space, which may be writable.