24.3.15 The Allocation Order of Bit-fields
The memory ordering of bit-fields into their storage unit is not specified by the ANSI C Standard. In the CCI, the first bit defined is the least significant bit of the storage unit in which it is allocated.
Example
The following example shows a structure containing bit-fields being defined.
struct {
unsigned lo : 1;
unsigned mid :6;
unsigned hi : 1;
} foo;
The bit-field lo is assigned the least significant bit of
the storage unit assigned to the structure foo. The bit-field
mid is assigned the next 6 least significant bits; and
hi, the most significant bit of that same storage unit byte.
Differences
This is identical with the previous operation of all compilers.
Migration to the CCI
No action required.