24.3.17 Floating-point Sizes
Under the CCI, floating-point types must not be smaller than 32 bits in size.
Example
The following example shows the definition for outY,
which is at least 32 bits in size.
float outY;
Differences
The 8-bit compilers have allowed the use of 24-bit float
and double types.
Migration to the CCI
When using 8-bit compilers, the float and
double type will automatically be made 32 bits in size once the CCI
mode is enabled. Review any source code that may have assumed a float or
double type and may have been 24 bits in size.
No migration is required for other compilers.