15.4 Specifying the Interrupt Vector
All 32-bit MCU devices have a primary interrupt vector table (IVT) at a default location. Some 32-bit MCU devices allow the IVT to be relocated/remapped using the IVTBASE register, some allow the IVT to be collapsed so that all peripheral interrupts are directed to a single trap vector, and some allow both (see Interrupt Vector Table.)
GOTO statement or creates the Reset Vector to the C run-time startup
module.For relocated IVTs, the interrupt vector will be allocated automatically by the linker to the correct IVT if standard naming convention is used. For example:
- function _T1Interrupt() would be assigned to the default table, named _ivt_0
- function _T1Interrupt_2() would be assigned to a table named _ivt_2
- function _PWM1Interrupt() would be assigned to both _ivt_0 and _ivt_2
When an interrupt function is defined, it appears in all IVTs, unless a number-specific version of that function has also been defined.