23.4 Operator
The @ operator may be used with other compilers to
indicate the desired memory location of an object. As the following table indicates, there
is no support for this syntax in MPLAB XC16, MPLAB XC-DSC or MPLAB XC32.
Using @ in a compatibility mode will generate a warning.
To prevent this warning from appearing again, use the reviewed address with the MPLAB C
__at() specifier instead.
Also, consider using the address attribute.
| IAR Compatibility Mode | |||
|---|---|---|---|
| Operator | XC16 | XC-DSC | XC32 |
@ | error | error | error |