6.6.11.10 -fstack-usage
Code compiled with -fstack-usage will generate an extra file that
specifies the maximum amount of stack used, on a per-function basis. The file has the
same basename as the target object file with a .su extension. Each line
of this file is made up of three fields:
- The name of the function.
- A number of bytes.
- One or more qualifiers:
static,dynamic,bounded.
The second field corresponds to the size of the known part of the function frame.
The qualifier static means that the function frame size is purely
static. It usually means that all local variables have a static size. In this case, the
second field is a reliable measure of the function stack utilization.
The qualifier dynamic means that the function frame size is not static.
It happens mainly when some local variables have a dynamic size. When this qualifier
appears alone, the second field is not a reliable measure of the function stack
analysis. When it is qualified with bounded, it means that the second
field is a reliable maximum of the function stack utilization.
See also: Static Stack Usage Analysis.