1.2.6 PRIME_Status Function
C
SYS_STATUS PRIME_Status(void)
Summary
Gets the current status of the PRIME Stack.
Description
This routine provides the current status of the PRIME Stack.
Precondition
PRIME_Initialize routine must have been called before.
Parameters
None.
Returns
SYS_STATUS_READY: Indicates that the PRIME Stack is ready and accepts requests for new operations.
SYS_STATUS_UNINITIALIZED: Indicates the PRIME Stack is not initialized.
SYS_STATUS_ERROR: Indicates the PRIME Stack is not initialized correctly.
SYS_STATUS_BUSY: Indicates the PRIME Stack is initializing.
Example
PRIME_STACK_INIT initData;
PRIME_Initialize(PRIME_INDEX_0, (SYS_MODULE_INIT *)&initData);
if (PRIME_Status() == SYS_STATUS_READY)
{
}
Remarks
None.