1.2.4 PRIME_Restart Function
C
void PRIME_Restart
(
uint32_t *primePtr,
uint8_t version
)
Summary
Restarts the PRIME Stack from a different location.
Description
This routine restarts the PRIME Stack from a different location.
Precondition
PRIME_Initialize routine must have been called before.
Parameters
| Param | Description |
|---|---|
| primePtr | Pointer to the PRIME API |
| version | PRIME version to run |
Returns
None.
Example
PRIME_STACK_INIT initData;
PRIME_Initialize(PRIME_INDEX_0, (SYS_MODULE_INIT *)&initData);
const PRIME_API *primeApiPtr = PRIME_SN_FWSTACK13_ADDRESS;
PRIME_Restart((uint32_t *)primeApiPtr, PRIME_VERSION_1_3);
Remarks
None.