1.5.5.4.28 SRV_FU_GetBitmap Function
C
uint16_t SRV_FU_GetBitmap(uint8_t *bitmap, uint32_t *numRxPages);
Summary
Gets the bitmap with the information about the status of each page of the image.
Description
This function is used to gets the bitmap with the information about the status of each page of the image.
Precondition
The SRV_FU_Initialize function should have been called before calling this function.
Parameters
| Parameters | Description |
|---|---|
| bitmap | Pointer to the bitmap information |
| numRxPages | Pointer to the number of pages received |
Returns
Size of bitmap. Maximum value is 1024 bytes. In case of returning 0, the bitmap buffer will be initialized internally in the PRIME Stack.
Example
uint8_t bitmap[1024]; uint32_t numPages = 0; SRV_FU_GetBitmap(&bitmap, &numPages);
Remarks
This function is called by the PRIME Stack.