3.3.6.1 TAP_RELEASE_TIMEOUT

The TAP_RELEASE_TIMEOUT parameter limits the amount of time allowed between the initial finger press and the liftoff. Exceeding this value will cause the firmware to not consider the gesture as a tap gesture. TAP_RELEASE_TIMEOUT needs to be lesser than the TAP_HOLD_TIMEOUT and SWIPE_TIMEOUT.

Unit: x10 ms

E.g., If TAP_RELEASE_TIMEOUT is configured as 3, then the user needs to finish tapping within 30 ms to qualify the gesture as tap.

ParameterRange
TAP_RELEASE_TIMEOUT 3 to 255