9.10.11 persistent

The persistent attribute specifies that the variable should not be initialized or cleared at startup. A variable with the persistent attribute could be used to store state information that will remain valid after a device Reset.

int last_mode __attribute__ ((persistent));

Persistent data is not normally initialized by the C/C++ runtime. However, from a cold-restart, persistent data may not have any meaningful value. This code example shows how to safely initialize such data:

#include <xc.h>

int last_mode __attribute__((persistent));

int main()
{
    if ((RCONbits.POR == 0) &&
        (RCONbits.BOR == 0)) {
      /* last_mode is valid */
   } else {
     /* initialize persistent data */
     last_mode = 0;
   }
}

This attribute can only be used in conjunction with a RAM resident object, i.e. not in FLASH.