9.10.18 space
(space)
Normally, the compiler allocates variables in general data space. The
space attribute can be used to direct the compiler to allocate a
variable in specific memory spaces. Memory spaces are discussed further in 11.1 Address Spaces The following
arguments to the space attribute are accepted:data– Allocate the variable in general data space. Variables in general data space can be accessed using ordinary C/C++ statements. This is the default allocation.xmemory– Allocate the variable in X data space. Variables in X data space can be accessed using ordinary C/C++ statements. An example ofxmemoryspace allocation is:int x[32] __attribute__ ((space(xmemory)));Depending on the device, other attributes may need to be used with
space()for xmemory, such as 9.10.2aligned (alignment).ymemory– Allocate the variable in Y data space. Variables in Y data space can be accessed using ordinary C/C++ statements. An example ofymemoryspace allocation is:int y[32] __attribute__ ((space(ymemory)));Depending on the device, other attributes may need to be used with
space()for ymemory, such as 9.10.2aligned (alignment).prog– Allocate the variable in program space in a section designated for executable code. This area of memory can be accessed with normal C/C++ statements.external– Allocate the variable in a user defined memory space. For complete details please see the 11.4 External Memory Access section.