6.7.12.3 -x
You can specify the input language explicitly with the -x option.
-x language
Specify explicitly the language for the following input files (rather than letting
the compiler choose a default based on the file name suffix). This option applies to
all following input files until the next -x option.
The following values are supported by the compiler: c,
c-header, cpp-output,
assembler, assembler-with-cpp.
-x none
Turn off any specification of a language, so that subsequent files are handled
according to their file name suffixes. This is the default behavior but is needed if
another -x option has been used.
For example:
-x assembler foo.asm bar.asm -x none main.c mabonga.s
Without the -x none, the compiler will assume all the input files
are for the assembler.