3.3 Curiosity Nano Base for Click boards™ Battery Charger
The board has an MCP73871-2CC battery charger for 4.20V Li-Ion/LiPo batteries with 2-pin JST B2B-PH connectors.
When connecting a battery with an external power source, the MCP73871 will charge the battery at a maximum current of 500 mA. When removing external power, the MCP73871 will source power from the battery to power the board. Customize the battery charge current by replacing resistor R7. The charge current follows the formula I = 1000V/R7. The default charge current is 500 mA.
The default input current is limited to 1.8A. If a battery is connected, the board’s current is prioritized, and any available current not required by the board will be used to charge the battery.
The input current limit can be changed by adjusting the configuration of J9, J10, J12, and J13, as shown in the table below.
| J9 | J10 | J12 | J13 | MCP73871 Current Limit [mA] |
|---|---|---|---|---|
| Open | Closed | Closed | Open | 80 to 100 |
| Open | Closed | Open | Closed | 80 to 100 |
| Closed | Open | Closed | Open | 1500 to 1800 |
| Closed | Open | Open | Closed | 400 to 500 (default) |
When the board is supplied by a battery, the only limitation regarding current is caused by the voltage regulators. The maximum output current from the two regulators, MCP16417 and MIC33050, is listed in the table below.
| Regulator | Input Voltage [V] | Output Current Limit [mA] |
|---|---|---|
| MCP16417 | 4.4 | 1000 |
| MCP16417 | 4.2 | 850 |
| MCP16417 | 3.6 | 600 |
| MCP16417 | 3.2 | 480 |
| MIC33050 | 5.0 | 600 |
If the Curiosity Nano Base for Click boards™ is powered by a Curiosity Nano microcontroller board using USB, the current limit is 500 mA.
If the battery is attached to the back of the board in the designated area, a thermistor can be mounted in footprint TH1 to enable the thermal protection feature in the MCP73871. Remove R21 when mounting the thermistor. As an example, using a 10-kΩ NTC with a β parameter of 3590 allows charging between approximately 4°C and 43°C.
Three status signals from the MCP73871 are connected to LEDs located at the upper edge of the board. The table below shows the different LED combinations.
| S1 | S2 | PS | Status |
|---|---|---|---|
| Off | Off | Off | Shutdown/no power |
| Off | Off | On | Shutdown/no battery connected |
| On | Off | On | Battery charging |
| Off | On | On | Battery charge complete |
| On | Off | Off | Low battery output |
| On | On | On | Temperature/timer fault |
| Designator | Default | Comment |
|---|---|---|
| J9 | Closed | MCP73871 current limit setting |
| J10 | Open | |
| J12 | Closed | |
| J13 | Open | |
| R20 | Not Mounted | Battery switch bypass, solder 0 Ohm to permanently connect the battery to the MCP73871 |
| R7 | Mounted, 2 kΩ | Sets the battery charge current |
| R21 | Mounted, 10 kΩ | Battery thermal protection feature of the MCP73871 |
| TH1 | Not Mounted |